PL.KP
Description
PL.KP sets the proportional gain of the position regulator PID loop.
General Information
Type |
NV Parameter |
Units |
(rev/s)/rev |
Range |
0 to 2,147,483.008 (rev/s)/rev |
Default Value |
100 rps/rev |
Data Type |
Float |
See Also |
|
Start Version |
M_01-00-00-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | No |
Index/Subindex | Object Start Version |
---|---|
3542h/0 | M_01-00-00-000 |
Related Topics