VL.KVFF

Description

This parameter sets the gain for the velocity feedforward (a scaled derivative of the position command is added to the velocity command value). The nominal feedforward value can be multiplied by this gain value.

This parameter is only used in the position mode (DRV.OPMODE = 2).

General Information

Type

R/W Parameter

Units

NA

Range

0.0 to 2.0

Default Value

0.0

Data Type

Float

See Also

VL.FF

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3407h/2

354Bh/0

M_01-00-00-000

Related Topics

"Velocity Loop"