MLAxisStop

Pipe Network motion icon

 Function Block - Stop with the specified deceleration.
This does not remove the input source, but does stop the drive from continuing to move.

  • This function stops any current Generator Motion.
  • It causes the axis to start ignoring any changes in Pipe position to be added into the reference position.
  • It decelerates, if moving, at a programmed rate.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Start

BOOL

FALSE, TRUE

N/A

No default

 

Deceleration

LREAL

No range

User unit/sec2

No default

 

See Set the Axis Block Position Units.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Becomes TRUE when the Axis is completely stopped.

GenPos

LREAL

 

User units

  • Corresponds to the Generator Position input to the axis at the time the stop is triggered.
  • See Axis Pipe Block about positions.

PipePos

LREAL

 

User units

  • Corresponds to the Pipe Position input to the axis at the time the stop is triggered.
  • See Axis Pipe Block about positions.

RealignPos

LREAL

 

User units

Realign Position is the Reference Position at which the stop is triggered.

  • The Realign Position is:
    • Obtained by converting the last value sent to the drive from drive interface units into user units.
    • Useful to return to the point at which the trajectory was abandoned or to realign the master to the slave.
  • See Axis Pipe Block about positions.

StopPos

LREAL

 

User units

Corresponds to the last Reference Position sent to the drive at the time when the Axis is completely stopped.

  • See Initialize and Start a Pipe Network.
  • It is functionally different than the Actual Position because that position is the drive position converted to user units.
  • The correct delta for the realign move to get in sync with the trajectory in order to realign the slave to the master is the current Reference Position minus the Stop Position for the realign move.
  • After stopping, if the axis is disabled and the motor position is manually altered, this distance must be considered when performing the realign.

Remarks

  • After stopping the drive, the motion must be restarted by realigning the Actual Position with the Reference Position.
  • When the stop occurs, the master keeps moving and the axis starts ignoring the Pipe Position value and begins a controlled stop based on the input parameters.
    See Axis Pipe Block for more information about Pipe Position.
    • At this point, any Axis Block level profile (issued from an FB like MLAxisAbs, MLAxisRel...) are aborted.
    • When the stop is complete, it is up to the application to decide how to move the axis, master, or both to a position where they can be realigned, and the master restarted.
  • The MLAxisReAlign function is used to move the axis to a restart position in order to enable synchronized machine motion to start again.
    • Once the realign function is successfully completed, the Pipe Position is again summed with the Generator Position to create the Reference Position.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Inst_MLAxisStop(PipeNetwork.AXIS1, bStop, 200000);
If Inst_MLAxisStop.Done Then
Axis1_PipePosition := Inst_MLAxisStop.PipePos;
Axis1_GeneratorPosition := Inst_MLAxisStop.GenPos;
Axis1_RealignPosition := Inst_MLAxisStop.RealignPos;
Axis1_StopPosition := Inst_MLAxisStop.StopPos;
End_if;

See Also

MLAxisReAlign