MLAxisWritePos

Pipe Network motion icon

 Function - Sets a new value to an axis’ current location.

  • If a convertor is not connected, zero Pipe Position and Pipe Offset.
  • If a convertor is connected (pipe active also), the pipe position and offset are left alone.
    • The actual position is then set equal to the target position, and the Zero Offset is adjusted for no motion.
    • The Reference position and Generator Positions are then realigned so that the new reference position creates no step in motion.
    • The lag between reference position and actual position is absorbed in the generator position.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

1 to 1024

N/A

No default

ID of the Axis block.

Position

LREAL

No range

User units

No default

The new value for the axis’ current location.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

  • Previous function name: MLAxisSetZero
  • After this function is called, the axis’ current location has a value equal to the Position argument.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

MLAxisWritePos(PipeNetwork.Axis1, 0) ;