MLMstReadAccel

Pipe Network motion icon

 Function - Gets the present acceleration value of a master block.

Inputs

Input

Data Type

Range

Unit

Default

Description

EN

BOOL

0 to 1

N/A

No default

Enables the FB to be executed.

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Master Block.

Outputs

Output

Data Type

Range

Unit

Description

OK

BOOL

FALSE, TRUE

N/A

Acceleration

LREAL

 

User unit/sec2

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

// Read the present  acceleration of a  Pipe Block named “MASTER”
MLMstReadAccel( PipeNetwork.MASTER );

See Also