MLMstRun

Pipe Network motion icon

 Function - Jogs at the specified speed.

Inputs

Input

Data Type

Range

Unit

Default

Description

EN

BOOL

FALSE, TRUE

N/A

No default

Enables the FB to be executed.

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Master Block.

Speed

LREAL

No range

User unit/sec2

No default

Defines the Master starting position when the motion starts.

See Set the Axis Block Position Units.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

MLMstRun( PipeNetwork.MASTER, 1250.0 );

See Also