MLSyncReadDeltaS

Pipe Network motion icon

 Function - Gets the output phasing value of a synchronizer block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

1 to 1024

N/A

No default

ID name of the Pipe Network Block.

Outputs

Output

Data Type

Range

Unit

Description

DeltaS

LREAL

 

User units

Present Delta Slope value.

Remarks

  • Output phasing is the distance or the slope the output takes to synchronize with the input when MLSyncStart block is executed.
  • It also affects the distance or the slope the output takes to de-synchronize with the input and come to a stop when MLSyncStop block is executed.

Figure 1: Get Output Phasing after MLSyncStart

Figure 2: Get Output Phasing after MLSyncStop

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

ActScope := MLSyncReadDeltaS( PipeNetwork.SYN );

See Also

MLSyncWriteDeltaS