AXIS#.WS.IMAX

Description

This parameter defines the maximum current used for wake and shake. If the selected current is too low, the minimum required movement may not occur. If the selected current is too high, the movement may be too fast (overspeed) or too large (over maximum movement).

The maximum of this parameter is the lower value of AXIS#.MOTOR.IPEAK and AXIS#.IPEAK. The default value of this parameter is the half of its maximum. This value depends on the specific application.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to (lower value of AXIS#.MOTOR.IPEAK and AXIS#.IPEAK) Arms

Default Value

(half of maximum) Arms

(missing or bad snippet)

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.IMAX

5013h

0dh

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6703

1

6703 (0x1a2f)

AXIS1.WS.IMAX

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.WS.IMAX

6703

Float

Read/Write

-