MLPipeCreate
Function - Create a new pipe object.
A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between.
-
-
- Pipes are created in the Pipe Network using the graphical engine.
- You do not have to add MLPipeCreate function blocks to their programs.
- The code with MLPipeCreate commands are automatically generated and called in a program with PipeNetwork(MLPN_CREATE_OBJECTS).
Inputs
|
Input |
Data Type See Data Types. |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Name |
STRING |
No range |
N/A |
No default |
Name for the newly created Pipe. |
Outputs
|
Output |
Data Type See Data Types. |
Range |
Unit |
Description |
|---|---|---|---|---|
|
ID |
DINT |
|
|
Assigned ID number of the created Pipe. |
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Create a new pipe
PipeAXIS1 := MLPipeCreate( 'PipeAXIS1' );
See Also
- MLPipeAct
- MLPipeAddBlock
- MLPipeDeact
- Pipe Network Functions for the PLC - MLPN_CREATE_OBJECTS