Retain Variables
A retain variable is a PLC variable which:
- Is non-volatile and stored in non-volatile controller memory (PCMM2G).
- When using the KAS Simulator, the retain variables are stored in a normal disk file.
- Is known by all programs (when its content is changed, the change is propagated to all equations in which this variable is used)
- Normally does not contain real-time critical data.
-
-
- Retain variables are saved when you stop the PLC.
- The next time the PLC starts, the retained values are used.
- Retains are auto-saved every two seconds.
- Changed variables stored in non-volatile memory are updated every two seconds.
- Unchanged variables are not updated.
Retain variables are typically used to store application-specific persistent state.
Example: Counting cutting edge cycles so maintenance is triggered after a preset number of operations:
- Retained Variable Initialization Behavior
- Best Practices Retained Variables
- Copy Retained Variable Values to Init Value
- Copy Retained Variables Values to Init Value from another Controller
Retained Variable Initialization Behavior
- On an Application Start, KAS initializes the retain variables using values stored in non-volatile memory (NVRAM).
- On an Application Cold Start, KAS initializes the retain variables using their Init values.
Warning - Dependency on Project Compatibility
- If the declaration of the retain variables is different between the non-volatile memory and the project, the retain variables are also reset to their Init values.
KAS Runtime determines compatibility using:
- The number of variables of each type.
- The length of a STRING type variables.
Non-volatile Storage Considerations
- The non-volatile memory size is hardware dependent.
- If the size of the retained variables is larger than the non-volatile storage space:
- An error is logged.
- Data is not stored in non-volatile memory.
- See NVRAM.
For the KAS Runtime Simulator, the retained variables are saved in a file in the project repository.
Actions that Reset Retained Values to Init Values
These changes invalidate existing retained data and reset to their Initial values.
- Change the type of a retain variable.
- Change the length of a string retain variable.
- Change the size of an array variable.
- Change any element of a structure variable.
- This includes adding new members.
-
-
Even small structural changes (e.g., adding one field) cause a complete reset of the affected retained variable.
See Also