Min_Profile_Velocity

Min_Profile_Velocity

Address: 4116 (1014H)
Type: WORD
Access: Read/Write
Unit: Hertz
Range: 0 to (150000*Motor_SPR / 65536)
Default Value: 0
Store Supported: Yes
Description: It sets the minimum motor velocity for the acceleration and deceleration ramp.
Notes:

This object can only be set with the motor at a standstill; this object cannot be higher than the Max_Profile_Velocity object.

If the value to be set is lower than the minimum value range, the minimum value is stored.

If the value to be set is higher than the maximum value range, the maximum value is stored.