Motor_SPR

Motor_SPR

Address: 4136 (1028H)
Type: WORD
Access: Read Only
Unit: --
Range: --
Default Value: --
Store Supported: No
Description:

Return the motor resolution as microsteps every motor turn. The value depends on objects Motor_Poles and Motor_Step_Angle

 If ‘Motor_Step_Angle’ value is different from 65535, the number of motor Increments per revolution are computed as follows :

 If the object Motor_Step_Angle is set to 65535, the Motor_SPR is considered = 65536 regardless of Motor_Poles.

Notes: --