Motor_Start_Delay

Motor_Start_Delay

Address: 8762 (223AH)
Type: DWORD
Access: Read/Write
Unit: µs
Range:

0 to 231

Default Value: 0
Store Supported: Yes
Description: It defines the delay on the motor start. This object can be used to have repetitive motor starts. Each time the motor has to start (MOVE command executed, or Motor_SYNC object written or Trigger Start input detected) Motor_Start_Delay microseconds are waited.
Notes: This object should not be used together with Motor_Start_Delay_Pulses object.