Brake_Control_Settings
| Index.Sub | 2C00.0H | ||||||||||||||||||||||||||||||||||||
| Data Type | Unsigned16 | ||||||||||||||||||||||||||||||||||||
| Access | Read/Write | ||||||||||||||||||||||||||||||||||||
| PDO Mappable | No | ||||||||||||||||||||||||||||||||||||
| Unit | -- | ||||||||||||||||||||||||||||||||||||
|
Range |
0 to 65535 |
||||||||||||||||||||||||||||||||||||
| Default Value | 0 | ||||||||||||||||||||||||||||||||||||
| Store Supported | Yes | ||||||||||||||||||||||||||||||||||||
| Description |
This object defines settings regarding the Brake Control functionality.
|
||||||||||||||||||||||||||||||||||||
|
Notes |
|
Bit Explanation
Automatic Brake Handling
When this bit is set to (1), the Automatic Brake Handling is enabled.
The digital output, defined by bit4÷bit7 and bit3 of Brake_Control_Settings object, is used for Brake Handling according to the rules defined by bit1 and bit2 of of Brake_Control_Settings object.
When this bit is reset (0) the Automatic Handling is disabled and settings of bit1÷bit7 are not considered.
Brake Control Type
Brake Control Type = 0
The brake is closed (active) if:
-
the drive is in one of the following states:
-
‘Switched On’ state or
-
‘Ready to switch on’ state or
-
‘Switch on disabled’ state or
-
‘Not ready to switch on’ state
-
‘Fault’ state.
-
-
the drive is in the ‘Operation enabled’ state and bit2 of Brake_Control_Settings object is equal to 1 and the digital output (used for the Brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object) is reset by B0_Digital_Outputs object (if bit3 = 0 of Brake_Control_Settings object) orB1_Digital_Outputs object (if bit3 = 1 of Brake_Control_Settings object).
The brake is opened (released) if:
-
the drive is in the ‘Operation enabled’ state and bit2 of Brake_Control_Settings object is equal to 0.
-
the drive is in the ‘Operation enabled’ state and bit2 of Brake_Control_Settings object is equal to 1 and the digital output (used for the Brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object) is set by B0_Digital_Outputs object (if bit3 = 0 of Brake_Control_Settings object) or B1_Digital_Outputs object (if bit3 = 1 of Brake_Control_Settings object).
Brake Control Type = 1
The brake is closed (active) if:
-
the drive is in the ‘Switched On’ state or ‘Ready to switch on’ state or ‘Switch on disabled’ state or ‘Not ready to switch on’ state or ‘Fault’ state.
-
the drive is in the ‘Operation enabled’ state and bit2 of Brake_Control_Settings object is equal to 1 and the digital output (used for the Brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object) is reset by B0_Digital_Outputs object (if bit3 = 0 of Brake_Control_Settings object) or B1_Digital_Outputs object (if bit3 = 1 of Brake_Control_Settings object).
-
if the drive is in the ‘Operation enabled’ state and the motor is at standstill and bit2 of Brake_Control_Settings object is equal to 0.
The brake is open (released) if:
-
if the drive is in the ‘Operation enabled’ state and bit2 of Brake_Control_Settings object is equal to 0 and the motor is running.
-
if the drive is in the ‘Operation enabled’ state and bit2 of Brake_Control_Settings object is equal to 1 and the digital output (used for the Brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object) is set by B0_Digital_Outputs object (if bit3 = 0 of Brake_Control_Settings object) or B1_Digital_Outputs object (if bit3 = 1 of Brake_Control_Settings object).
Brake Digital Output use Mode:
-
When this bit is set (1), according to the Brake Control Type (bit1 of Brake_Control_Settings object), the state of Digital Output (used for the Brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object), can be changed by B0_Digital_Outputs object (if bit3 = 0 of Brake_Control_Settings object) or B1_Digital_Outputs object (if bit3 = 1 of Brake_Control_Settings object).
-
When this bit is reset (0) the state of Digital Output (used for the Brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object) can not be changed by B0_Digital_Outputs object (if bit3 = 0 of Brake_Control_Settings object) or B1_Digital_Outputs object (if bit3 = 1 of Brake_Control_Settings object).
Brake Digital Output Bank:
-
When this bit is set (1) the Digital Output, used for the brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object, is related to digital outputs of Bank#1.
-
When this bit is set (0) the Digital Output, used for the brake and defined by bit4÷bit7 and bit3 of Brake_Control_Settings object, is related to digital outputs of Bank#0.
Brake Digital Output:
-
The bit4÷bit7 define Digital output used for the Brake. It can be related to digital outputs of Bank#0 (if bit3 = 0 of Brake_Control_Settings object) or Bank#1 (if bit3 = 1 of Brake_Control_Settings object).
-
If the Digital Output used for the Brake is B0_OUT0 (digital output #0 of Bank#0) or B0_OUT1 (digital output #1 of Bank#0) is necessary to reset (0) the bit7 of Drive_Working_Settings object.