Feedback_Ki
Index.Sub | 2230.0BH |
Data Type | Unsigned32 |
Access | Read/Write |
PDO Mappable | No |
Unit | -- |
Range |
Unsigned32 |
Default Value |
1000 |
Store Supported | Yes |
Description | This value is used for Closed Loop feature and defines the integral gain of PID’s regulator. The value has to be adjust to reduce the position error (Feedback_Actual_Position_Error) or velocity error (Feedback_Actual_Velocity_Error) at the end of acceleration ramp or deceleration ramp. |
Notes |
A value too high could introduce motor’s vibration. |