Feedback_Status
Index.Sub | 2230.18H | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Data Type | Unsigned16 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Access | Read Only | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
PDO Mappable | No | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Unit | -- | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Range |
Unsigned16 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Default Value | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Store Supported | Yes | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Description |
This object is used for Closed Loop functionality and returns the Feedback Status.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Notes |
(1) This bit is available only with firmware version V02r74 or superior. (2) This bit is available only with firmware version V02r82 or superior. |