IL.FOLDFTHRESHU

Description

IL.FOLDFTHRESHU is the fault level of the current foldback algorithm. The value of IL.FOLDFTHRESH is the minimum of DRV.IPEAK, MOTOR.IPEAK, and IL.FOLDFTHRESHU.

General Information

Type

NV Parameter

Units

Arms

Range

0 to 500 Arms

Default Value

Drive peak current (DRV.IPEAK)

Data Type

Float

See Also

IL.FOLDFTHRESH, Foldback

Start Version

M_01-00-00-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3421h/0 M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2219 DWord Yes
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
220 4 Byte Signed Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

438

No 32 bit Yes M_01-03-00-000

Related Topics

"Current Loop"