AXIS#.SAFEPARAM.SLS_#.TIMETOVELMONITORING
Description
Indicates the maximum time before starting the velocity monitoring of the Safely Limited Speed (SLS) safety function. If the velocity is not below the limit when this time elapsed then the function is faulted and it activates the configured fault reaction.
This value is t_SLS in the following diagram:
Context
For complete SLS information refer to SLS (Safely Limited Speed).
Related safety parameters:
- AXIS#.SAFE.SLS_#.INTERNALSTATE
- AXIS#.SAFEPARAM.SLS_#.DECLIMIT
- AXIS#.SAFEPARAM.SLS_#.DECMONITOREN
- AXIS#.SAFEPARAM.SLS_#.FAULTREACTION
- AXIS#.SAFEPARAM.SLS_#.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SLS_#.FSOE
- AXIS#.SAFEPARAM.SLS_#.SAFEINPUT
- AXIS#.SAFEPARAM.SLS_#.TIMEFORVELINLIMITS
- AXIS#.SAFEPARAM.SLS_#.VELLIMIT
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
Type |
Read/Write |
Units |
Milliseconds |
Range |
[2, 60000] |
Default Value |
2 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.SAFEPARAM.SLS_1.TIMETOVELMONITORING |
315ch |
04h |
Unsigned16 |
- |
- |
Read/Write |
No |
AXIS1.SAFEPARAM.SLS_2.TIMETOVELMONITORING |
315dh |
04h |
Unsigned16 |
- |
- |
Read/Write |
No |
AXIS1.SAFEPARAM.SLS_3.TIMETOVELMONITORING |
315eh |
04h |
Unsigned16 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_1.TIMETOVELMONITORING |
325ch |
04h |
Unsigned16 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_2.TIMETOVELMONITORING |
325dh |
04h |
Unsigned16 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_3.TIMETOVELMONITORING |
325eh |
04h |
Unsigned16 |
- |
- |
Read/Write |
No |