AXIS#.SAFEPARAM.SLS_#.FSOE
Description
Indicates if the Safely Limited Speed (SLS) function can be activated through FSoE. This parameter can only set to “Used” when FSoE is activated (SAFEPARAM.SAFEFIELDBUS.ACTIVATION is set to 1 – “Activated”).
Value | Description |
---|---|
0 |
Not used |
1 |
Used |
Context
For complete SLS information refer to SLS (Safely Limited Speed).
Related safety parameters:
- AXIS#.SAFE.SLS_#.INTERNALSTATE
- AXIS#.SAFEPARAM.SLS_#.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SLS_#.DECLIMIT
- AXIS#.SAFEPARAM.SLS_#.DECMONITOREN
- AXIS#.SAFEPARAM.SLS_#.TIMEDELAYDECMONITORING
- AXIS#.SAFEPARAM.SLS_#.TIMETOVELMONITORING
- AXIS#.SAFEPARAM.SLS_#.FAULTREACTION
- AXIS#.SAFEPARAM.SLS_#.SAFEINPUT
- AXIS#.SAFEPARAM.SLS_#.TIMEFORVELINLIMITS
- AXIS#.SAFEPARAM.SLS_#.VELLIMIT
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0, 1 |
Default Value |
0 (Not used) |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.SAFEPARAM.SLS_1.FSOE |
315ch |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS1.SAFEPARAM.SLS_2.FSOE |
315dh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS1.SAFEPARAM.SLS_3.FSOE |
315eh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_1.FSOE |
325ch |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_2.FSOE |
325dh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_3.FSOE |
325eh |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |