AXIS#.SAFEPARAM.SLS_#.TIMEDELAYDECMONITORING

Description

Indicates the delay before starting the deceleration monitoring. The delay starts elapsing when Safely Limited Speed (SLS) is activated. When it finally elapses, the monitoring is started. This parameter can only be used when the deceleration monitoring is enabled in the safety parameters (see AXIS#.SAFEPARAM.SLS_#.DECMONITOREN).

 

This value is t_D_SLS in the following diagram:

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[1, 60000]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.TIMEDELAYDECMONITORING

315ch

05h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.TIMEDELAYDECMONITORING

315dh

05h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.TIMEDELAYDECMONITORING

315eh

05h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.TIMEDELAYDECMONITORING

325ch

05h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.TIMEDELAYDECMONITORING

325dh

05h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.TIMEDELAYDECMONITORING

325eh

05h

Unsigned16

-

-

Read/Write

No