AXIS#.SAFEPARAM.SLS_#.VELLIMIT
Description
Indicates the velocity limit of the Safely Limited Speed (SLS) safety function.
This value is n_SLS in the following diagram:
Context
For complete SLS information refer to SLS (Safely Limited Speed).
Related safety parameters:
- AXIS#.SAFE.SLS_#.INTERNALSTATE
- AXIS#.SAFEPARAM.SLS_#.DECLIMIT
- AXIS#.SAFEPARAM.SLS_#.DECMONITOREN
- AXIS#.SAFEPARAM.SLS_#.FAULTREACTION
- AXIS#.SAFEPARAM.SLS_#.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SLS_#.FSOE
- AXIS#.SAFEPARAM.SLS_#.SAFEINPUT
- AXIS#.SAFEPARAM.SLS_#.TIMEDELAYDECMONITORING
- AXIS#.SAFEPARAM.SLS_#.TIMEFORVELINLIMITS
- AXIS#.SAFEPARAM.SLS_#.TIMETOVELMONITORING
- AXIS#.SAFEPARAM.SLS_#.VELLIMIT
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
Type |
Read/Write |
Units |
Depends on user units |
Range |
[1, 2^31-1] |
Default Value |
1 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.SAFEPARAM.SLS_1.VELLIMIT |
315ch |
07h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS1.SAFEPARAM.SLS_2.VELLIMIT |
315dh |
07h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS1.SAFEPARAM.SLS_3.VELLIMIT |
315eh |
07h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_1.VELLIMIT |
325ch |
07h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_2.VELLIMIT |
325dh |
07h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SLS_3.VELLIMIT |
325eh |
07h |
Unsigned32 |
- |
- |
Read/Write |
No |