AXIS#.SAFEPARAM.SLS_#.DECMONITOREN

Description

Indicates if the deceleration monitoring is enabled for the Safely Limited Speed (SLS) safety function.

Value Description

0

Disabled (Default)

1

Enabled

 

Parameters Editor with the Deceleration Monitoring options shown and circled

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Disabled)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.DECMONITOREN

315ch

08h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.DECMONITOREN

315dh

08h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.DECMONITOREN

315eh

08h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.DECMONITOREN

325ch

08h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.DECMONITOREN

325dh

08h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.DECMONITOREN

325eh

08h

Unsigned8

-

-

Read/Write

No