AXIS#.SAFEPARAM.SSR_#.DECMONITOREN

Description

Indicates if the deceleration monitoring is enabled for the Safe Speed Range (SSR) safety function.

Value Description

0

Disabled (Default)

1

Enabled

 

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Disabled)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.DECMONITOREN

3161h

06h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.DECMONITOREN

3162h

06h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.DECMONITOREN

3163h

06h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.DECMONITOREN

3261h

06h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.DECMONITOREN

3262h

06h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.DECMONITOREN

3263h

06h

Unsigned8

-

-

Read/Write

No