AXIS#.SAFEPARAM.SSR_#.FSOE

Description

Indicates if the Safe Speed Range (SSR) function can be activated through FSoE. This parameter can only be set to “Used” when FSoE is activated (SAFEPARAM.SAFEFIELDBUS​.ACTIVATION is set to 1 – “Activated”).

Value Description

0

Not used

1

Used

 

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Not used)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.FSOE

3161h

03h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.FSOE

3162h

03h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.FSOE

3163h

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.FSOE

3261h

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.FSOE

3262h

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.FSOE

3263h

03h

Unsigned8

-

-

Read/Write

No