AXIS#.SAFEPARAM.SSR_#.TIMETOVELMONITORING

Description

Indicates the maximum time to start the velocity monitoring for the Safe Speed Range (SSR) safety function. If the velocity is still not in range after this time, the function will be faulted and activates its configured fault reaction

 

This value is t_SSR in the following diagram:

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[1, 60000]

Default Value

2

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.TIMETOVELMONITORING

3161h

04h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.TIMETOVELMONITORING

3162h

04h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.TIMETOVELMONITORING

3163h

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.TIMETOVELMONITORING

3261h

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.TIMETOVELMONITORING

3262h

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.TIMETOVELMONITORING

3263h

04h

Unsigned16

-

-

Read/Write

No