MC_EStop
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
En |
BOOL |
FALSE, TRUE |
N/A |
No default |
A positive Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. transition of this input causes an E-stop on the specified axis. |
Axis |
AXIS_REF |
1, 256 |
N/A |
No default |
The AXIS_NUM element of the AXIS_REF structure.
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
OK |
BOOL |
FALSE, TRUE |
N/A |
|
Remarks
-
-
This function or function block A function block groups an algorithm and a set of private data. It has inputs and outputs. returns cached data.
See Program a Multi-Core Controller.
- See Function Blocks - General Rules about how inputs and outputs work.
- Call MC_EStop to generate an emergency stop for an axis.
- Call MC_ResetError to reset New start of the microprocessor. the emergency stop.
- Actions of an E-stop:
- Stops motion interpolation.
- Clears all moves from the queue (active and next).
- Changes the axis state to ErrorStop.
- See PLCopen State Machine for more information.
- Request the drive In electrical engineering, a drive is an electronic device to provide power to a motor or servo. Control device for regulating the speed, torque and position of a motor. A unit controlling a motor using the current and timing in its coils. to open the position loop and disable Removal of the ENABLE signal. Disables power stage. the drive.
- The E-stop remains in effect until the application calls MC_ResetError to reset the E-stop.
Figure 1: MC_EStop
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_EStop ST Structured text - A high-level language that is block structured and syntactically resembles Pascal. example *)
ON EStopButton DO
MC_EStop( Axis1 );
MC_EStop( Axis2 );
END_DO;
See Also