MC_Halt
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
Execute |
BOOL |
0, 1 |
N/A |
No default |
On the rising edge The transition of a digital signal from low to high. AKA: positive edge., request to queue the move. |
Axis |
AXIS_REF |
1, 256 |
N/A |
No default |
Name of a declared instance of the AXIS_REF library function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances..
|
Deceleration |
LREAL |
No range |
User unit/sec2 |
No default |
Trapezoidal: Deceleration rate. S-curve: Unused. |
LREAL |
No range |
User unit/sec3 |
No default |
Trapezoidal: 0 (zero). S-curve: Constant jerk. |
|
BufferMode |
SINT |
0, 5 |
N/A |
No default |
|
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
Done |
BOOL |
No range |
N/A |
Indicates the move completed successfully. |
Busy |
BOOL |
No range |
N/A |
High from the moment the Execute input goes high until the time the move is ended. |
Active |
BOOL |
No range |
N/A |
Indicates this move is the Active move. |
CommandAborted |
BOOL |
No range |
N/A |
Indicates the move was aborted. |
Error |
BOOL |
No range |
N/A |
Indicates either:
|
ErrorID |
INT |
No range |
N/A |
Indicates the error if the Error output is set to TRUE. |
Remarks
-
- This function block starts a motion-related action and stores data for calculations and error checking.
See Call Function Blocks Multiple Times in the Same Cycle if using a dual-core controller.
- See Function Blocks - General Rules about how inputs and outputs work.
- It is a queued single-axis move.
- The move is complete when the axis reaches zero velocity.
- It is typically used with Abort at the BufferMode input to terminate a move.
- See MC_Stop to execute a stop that cannot be aborted.
- See Main about how this function is used in the Hole punch project.
Figure 1: MC_Halt
Time Diagram
This example shows the behavior in combination with a MC_MoveVelocity.
- A rotating axis is ramped The gradual acceleration and deceleration of a stepping motor. This is essential if performance beyond the start/stop range is required. The slope of the ramp is a function of screw pitch, load, drive voltage and design, and motor. down with FB2 MC_Halt.
- Another motion command overrides the MC_Halt command.
- MC_Halt allows this, in contrast to MC_Stop.
- The axis can accelerate again without reaching standstill.
Figure 2: Time Diagrams: First and Second FBs
Figure 3: Time Diagram
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
(* MC_Halt ST example *)
Inst_MC_Halt( HaltReq, Axis1,100.0, 100.0, 0 );
//Inst_MC_Halt is an instance of MC_halt function block
HaltComplete := Inst_MC_Halt.Done; //store Done output into user defined variable
See Also