MLSyncReadDeltaS
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Gets the output phasing value of a synchronizer Combines an axis or axes group (as slave) with an axis as master. The slave executes its path with synchronization to the progress of the master. This is linked to a one dimension source for synchronization. block.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Pipe Network Block. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
DeltaS |
LREAL |
|
User units |
Present Delta Slope value. |
Remarks
- Output phasing is the distance or the slope the output takes to synchronize with the input when MLSyncStart block is executed.
- See the Figure: "Get Output Phasing after MLSyncStart" image.
- It also affects the distance or the slope the output takes to de-synchronize with the input and come to a stop when MLSyncStop block is executed.
- See the Figure: "Get Output Phasing after MLSyncStop" image.
Figure 1: Get Output Phasing after MLSyncStart
Figure 2: Get Output Phasing after MLSyncStop
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
ActScope := MLSyncReadDeltaS( PipeNetwork.SYN );
See Also