AXIS#.IL.IWCMD

Description

AXIS#.IL.IWCMD reports the actual phase W current command after limits have been applied to AXIS#.IL.IUCMDU and AXIS#.IL.IVCMDU. It is in use when AXIS#.OPMODE = 0 (Torque mode) and AXIS#.IL.CMDMODE = 1 (Phase Current mode).

Versions

Action Version Notes
Implemented 02-07-03-000  

General Information

Type Read only
Units Arms
Range Same as AXIS#.IL.IUCMDU range
Default Value N/A
Data Type Float
See Also AXIS#.IL.CMDMODE, AXIS#.IL.IUCMDU, AXIS#.IL.IVCMDU, AXIS#.IL.SETCMD
Stored in Non-Volatile Memory N/A

Variants Supported

All variants are supported.

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5836

1

5836 (0x16cc)

AXIS1.IL.IWCMD

Signed32

Read Only

Yes

71372

2

5836 (0x16cc)

AXIS2.IL.IWCMD

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.IWCMD

5836

Float

Read Only

-

Related Topics

Current Loop