AXIS#.SAFE.SLP_#.INTERNALSTATE
Description
Indicates the internal state of the Safely Limited Position (SLP) function state machine.
|
Value |
Description |
|---|---|
|
0 |
Not Running |
|
1 |
Monitoring |
|
2 |
Fault Reaction |
|
3 |
Delay Before Monitoring |
State Machine Diagram
Context
For complete SLP information refer to SLP (Safely Limited Position).
- AXIS#.SAFE.SLP_#.ACTIVE
- AXIS#.SAFEPARAM.SLP_#.FAULTREACTION
- AXIS#.SAFEPARAM.SLP_#.FSOE
- AXIS#.SAFEPARAM.SLP_#.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SLP_#.POSLOWERLIMIT
- AXIS#.SAFEPARAM.SLP_#.POSUPPERLIMIT
- AXIS#.SAFEPARAM.SLP_#.SAFEINPUT
- AXIS#.SAFEPARAM.SLP_#.TIMEDELAYMONITORING
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0, 1, 2, 3 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |