ASCII Objekt-Reference 

 

Home 

Screen page "Homing" 

The reference traverse (homing) is an absolute task, that is used to zero the drive for subsequent positioning operations. You can choose between various types of homing. 

After homing, the drive reports "InPosition" and then enables the position controller in the servo amplifier. 

warning_r_general_14.JPG  

Take care that the zero point of the machine (reference point) is in a position that permits the subsequent positioning operations. The software limit-switches that were set as parameters may be ineffective. The axis could move on to the hardware limit-switch or even the mechanical stop. There is a risk of damage. 

If the reference point (zero point of the machine) is approached with excessive velocity, for instance because of high moments of inertia, it may be overshot and, in the worst case, move on to the hardware limit-switch or even the mechanical stop. There is a risk of damage. 

The position controller cannot be operated without first making a reference traverse (homing).
A homing/reference traverse must be made after the 24V auxiliary voltage has been switched on.
The start signal must not be removed during homing. 

The start signal must remain present until the "InPosition" message appears. The SW-enable is set automatically when homing starts. Homing will only be started in OPMODE 8. However, the SW-enable is set in all OPMODES. The drive can therefore be accelerated by an analog setpoint that is applied, if the START command is executed in OPMODES1 or 3. 



Start 

ASCII: MH 

Default: - 

valid for OPMODE 8 

Radio button to start homing. 



Stop 

ASCII: STOP 

Default: - 

valid for all OPMODES 

Radio button to stop (cancel) the homing. The SW-enable remains set! 



Reference traverse 

ASCII: NREF 

Default: 0 

valid for OPMODE 8 

You can choose which type of reference traverse should be performed. A preset zero-point offset (screen page "Encoder" is taken into account for the position output and display.
Exception: Homing 5 — in this case the true current position is displayed.
You can shift the zero-crossing point of the motor shaft within one turn, at will, by using the "NI offset" parameter (screen page "Encoder"). 

Zero-point recognition: the reference point is set to the first zero-crossing point of the feedback unit (zero mark) after recognition of the reference switch transition. Two-pole resolvers and all encoders have just one zero-crossing per turn, so the positioning at the zero mark is unambiguous within a motor turn. For 4-pole resolvers there are two zero-crossings per turn, and for 6-pole resolvers there are three zero-crossings.
If the transition of the reference switch lies very close to the zero-crossing point of the feedback unit, then the positioning to the zero mark can vary by one motor turn. 

0info_15.JPG  

The repetition accuracy of homing operations that are made without zero-point recognition depends on the traversing speed and the mechanical design of the reference switch or limit-switch. 

Homing 0 

Sets the reference point to the setpoint position (the following error is lost). 

Homing 1 

Traverse to the reference switch with zero-mark recognition. 

In this case, a reference traverse can also be made without hardware limit-switches. The precondition is one of the initial situations shown below: 

 

negative traverse,
positive rotation 

negative traverse,
negative rotation 

 

A0243-15  

Homing 2 

Move to hardware limit-switch, with zero-mark recognition. The reference point is set to the first zero-crossing of the feedback unit (NM, zero mark) beyond the limit-switch. 

Homing 3 

Move to reference switch, without zero-mark recognition. The reference point is set to the transition of the reference switch. 

Homing 4 

Move to hardware limit-switch, without zero-mark recognition. The reference point is set to the transition of the hardware limit-switch. 

Homing 5 

Move to the next zero-mark of the feedback unit. The reference point is set to the next zero-mark of the feedback unit. 

Homing 6 

Sets the reference point to the actual position (the following error is not lost). 

Homing 7 

Move to mechanical stop, with zero-mark recognition. The reference point is set to the first zero-crossing of the feedback unit (NM, zero mark) beyond mechanical stop.
The pulse current is set by the parameter REF.-IPEAK on the screen page "Current controller". 

Homing 8 

Drives to an absolute SSI position. At the start of the homing run, a position is read in from the SSI input (GEARMODE=7), converted according to the scaling factors GEARI and GEARO and the reference offset, and then used a the target position. 

On the following pages you can find the paths traversed during homing types 1 to 5 for every
possible initial situation (positive rotation, negative and positive directions of motion). 

The meanings of the abbreviations in the drawings are: 

N 

limit-switch NSTOP 

P 

limit-switch PSTOP 

SP 

start position 

R 

reference switch 

vref 

preset velocity 

NM 

zero mark of the resolver 



Homing 1 

warning_r_general_16.JPG  

Warning!
Before starting homing, check the safety of the system, since the load may move, even if the limit-switches are disconnected or defective.
The
limit-switch functions 2, PSTOP and 3, NSTOP must be activated to achieve the full homing functionality. 

Homing with reference switch, negative direction of motion, positive rotation, with zero-mark 

A0243-16


Homing with reference switch, positive direction of motion, positive rotation, with zero-mark 

A0243-17


Homing 2 

warning_r_general_17.JPG  

Warning!
Hardware limit-switches must be present and connected.
The
limit-switch functions 2, PSTOP and 3, NSTOP must be switched on. 

Homing without reference switch, negative direction of motion, positive rotation, with zero-mark 

A0243-18


Homing without reference switch, positive direction of motion, positive rotation, with zero-mark 

A0243-19



Homing 3 

warning_r_general_18.JPG  

Warning!
Before starting homing, check the safety of the system, since the load may move, even if the limit-switches are disconnected or defective.
The
limit-switch functions 2, PSTOP and 3, NSTOP must be activated to achieve the full homing functionality. 

Homing with reference switch, negative direction of motion, positive rotation, without zero-mark 

A0243-10


Homing with reference switch, positive direction of motion, positive rotation, without zero-mark 

A0243-21



Homing 4 

warning_r_general_19.JPG  

Warning!
Hardware limit-switches must be present and connected.
The
limit-switch functions 2, PSTOP and 3, NSTOP must be switched on. 

Homing without reference switch, negative direction of motion, positive rotation, without zero-mark 

A0243-22


Homing without reference switch, positive direction of motion, positive rotation, without zero-mark 

A0243-23



Homing 5 

0info_20.JPG  

Behavior for successively repeated starts of Homing 5:
The position controller can only hold the motor in the zero position by passing the zero mark by ± 1 count. On a repeated start of Homing 5, depending on the position (1 count in advance of or 1 count behind the zero-mark) and the count direction, the movement may be a full motor turn!
 

Homing without reference switch, negative direction of motion, positive rotation, with zero-mark 

a0243-24


Homing without reference switch, positive direction of motion, positive rotation, with zero-mark 

a0243-13



Homing 7 

warning_r_general_21.JPG  

Warning! 

Using this type of homing run can damage the mechanical stop on the machine. The peak current Ipeak and the continuous current Irms are limited for the duration of the homing run. 

A more severe limiting of the current is possible. (see parameter Ref.-Ipeak). 

Homing to mechanical stop, negative direction of motion, positive rotation, with zero-mark 


A0243-27


Homing to mechanical stop, positive direction of motion, positive rotation, with zero-mark 


A0243-28




Direction of motion 

ASCII: DREF 

Default: 0 

valid for OPMODE 8 

Determines the direction of motion for homing. The setting "distance-dependent" is only relevant for Homing 5 (within one turn). In this case, the direction is chosen to give the shortest distance to the zero-mark. This parameter also defines the direction of motion for a Modulo type of axis.
 


v for homing 

ASCII: VREF 

Default: 0 

valid for OPMODE 8 

Determines the velocity for the homing operation. The sign is automatically fixed by the direction of motion that is selected. The dimension is set by VUNIT .
 


Accel. ramp 

ASCII: ACCR 

Default: 10 ms 

valid for OPMODE 8 

The acceleration ramp for the homing operation. The dimension is set by ACCUNIT. Entry e.g. in milliseconds (1 ... 32767 ms). The ramp is also valid for constant velocity mode.
 


Decel. ramp 

ASCII: DECR 

Default: 10 ms 

valid for OPMODE 8 

The deceleration (braking) ramp for homing. The dimension can be set by ACCUNIT. Entry e.g. in milliseconds (1 ... 32767 ms). The ramp is also valid for constant velocity mode. This deceleration ramp is only used if the operating mode allows it. For homing to a hardware limit-switch, the emergency ramp is used.
 


Offset 

ASCII: ROFFS 

Default: 0 

valid for OPMODE 8 

With the reference offset you can assign an absolute position value other than 0 to the reference point. With an offset for the reference position you are not actually making a physical change, but the offset is used as a reference value within the position control of the servo amplifier. Homing to the reference switch will then not finish at zero, but at the preset reference offset value. The reference offset must be set before homing is started. The dimension is set by PUNIT. An alteration of the offset only takes effect after a new homing operation.
The parameter "
Resolution" must be set correctly for your application. 

Jog mode 

Jog mode is defined as an endless motion at a constant velocity. This type of operation can be started without a reference point being set. The hardware limit-switches are monitored. Software limit-switches are only monitored if a reference point has been set. Acceleration and deceleration ramps are taken from the settings for homing. 

0info_22.JPG  

When the function "Jog mode" is started, the SW-enable is set automatically. The Function "Jog mode" is only started in OPMODE 8. However, the SW-enable is set in all OPMODES. The drive can therefore be accelerated by an analog setpoint that is applied, if the START command is executed in OPMODES1 or 3. 



v 

ASCII: VJOG 

Default: 0 

valid for OPMODE 8 

Determines the velocity for jog mode. The sign that is entered determines the direction of movement. Before starting the jog mode, the velocity value must be taken on. The dimension is set by VUNIT .
 


F4 

ASCII: MJOG 

Default: - 

valid for OPMODE 8 

Start the jog mode by pressing the function key F4. The drive moves with the preset velocity in the direction, which is indicated by the sign of the velocity for the jog mode "v", as long as the function key is pressed. If a communication error occurs while pressing the button, the drive stops with the emergency deceleration ramp.