TxPDO - AKD-N Drive CANopen Objects
This table identifies:
- The CANopen objects required by the motion engine and function blocks.
- Whether the objects are available in the default PDO.
- Their corresponding drive parameter.
-
-
Review the table to verify the objects needed by the features the application uses are included in the PDO selection.
|
TxPDO - AKD-N Drive CANopen Objects |
|||||
|---|---|---|---|---|---|
|
Index - subindex |
Object Name |
Required |
Associated ML FB |
Associated MC FB |
Associated Drive Parameter |
|
0x6041:0 |
Yes |
N/A |
N/A |
N/A |
|
|
0x6063:0 |
Position Actual Value |
No |
|
PL.FB
|
|
|
0x606C:0 |
Velocity actual value |
No |
|
|
VL.FB
|
|
0x6077:0 |
Torque actual value |
No |
|
|
IL.FB
|
|
0x20A5:0 |
Latch status word |
No |
|
CAPx.STATE |
|
|
0x20A6:0 |
Latch position |
No |
|
|
|
|
0x60FD:0 |
Digital inputs Used by Onboard I/O mappings |
No |
N/A |
N/A |
DIN.STATES
|
|
0x60F4 |
Following error |
No |
|
|
PL.ERR
|