TxPDO - KED Drive CANopen Objects

This table identifies:

  • The CANopen objects required by the motion engine and function blocks.
  • Whether the objects are available in the default PDO.
  • Their corresponding drive parameter.

  • Review the table to verify the objects needed by the features the application uses are included in the PDO selection.

TxPDO - KED Drive CANopen Objects

Index - subindex

Object Name

Required

Associated ML FB

Associated MC FB

Associated Drive Parameter

0x6041:0

Status word Axis

Yes

Needed for the servo axis mapped to the drive to work properly.

Needed for the servo axis mapped to the drive to work properly.

 

0x6064:0

Position Actual Value Axis

Yes

Needed for the servo axis mapped to the drive to work properly.

Needed for the servo axis mapped to the drive to work properly.

 

0x6077:0

Torque actual value Axis

No

MLAxisReadTq

 

0x60B9:0

Touch Probe Status

No

 

0x60D1:0

Touch Probe 1

Time Stamp Positive Value

No

 

0x60D4:0

Touch Probe 2

Time Stamp Positive Value

No

 

0x60E4:3

3rd Additional

Position Actual Value

No

MLSmpConECAT

For a digitizing axis

 

0x60E4:4

4th Additional

Position Actual Value

No

MLSmpConECAT

For a digitizing axis

 

0x60E4:5

5th Additional

Position Actual Value

No

MLSmpConECAT

For a digitizing axis

 

0x60F4:0

Following error

Actual value

No

MLAxisReadFEUU