Import or Export Methods

KAS-IDE provides import and export capabilities to simplify the reuse, sharing, backup, and migration of User-Defined Function Blocks (UDFBs) and their methods between projects.

  • Individual methods can be exported and imported independently.
    • This allows commonly used functionality to be reused across multiple UDFBs and applications.
  • Entire UDFBs can also be exported together with all associated methods.
    • This preserves the complete function block structure and implementation.

The import/export functionality can be used to:

  • Reuse methods across multiple projects.
  • Share methods or UDFBs with other developers.
  • Create reusable libraries of application-specific functionality.
  • Back up custom UDFBs and methods.
  • Transfer UDFBs and methods between projects.

KAS-IDE supports these export formats:

Object

File Format

Contents

Method

.XK5

Single method, including interface definitions and implementation.

UDFB

.ZIP

Parent UDFB together with all associated methods and their implementations.

See: