AXIS#.MOTOR.IDMAX
Description
This parameter is supported for IPM motors (AXIS#.MOTOR.TYPE = 6). AXIS#.MOTOR.IDMAX is the maximum motor winding current in the direct (non-torque producing) axis.
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET=1 and motor memory version is 0.3 or greater. This parameter can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 6
Context
For more information see Motor.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Arms |
Range |
0.2 to 1000 |
Default Value |
0.5 * AXIS#.MOTOR.IPEAK |
Data Type |
Float |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.MOTOR.IDMAX |
500bh |
27h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
AXIS2.MOTOR.IDMAX |
510bh |
27h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
6232 |
1 |
6232 (0x1858) |
AXIS1.MOTOR.IDMAX |
Unsigned32 |
Read Only |
Yes |
71768 |
2 |
6232 (0x1858) |
AXIS2.MOTOR.IDMAX |
Unsigned32 |
Read Only |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.MOTOR.IDMAX |
6232 |
Float |
Read Only |
- |