|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
Hz |
|
Range |
0 to 250 Hz |
|
Default Value |
0 Hz |
|
Data Type |
Float |
|
See Also |
PL.KP, PL.KD |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3480h/0 |
M_01-00-00-000 |
Description
PL.KI sets the integral gain of the position regulator PID"Proportional-Integral-Derivative" A PID controller is a generic control-loop feedback mechanism widely used in industrial control systems. An "error" occurs when an event or a disturbance triggers off a change in the process variable. A PID controller attempts to correct the error between a measured process variable and a desired setpoint by calculating and then outputting a corrective action that can adjust the process accordingly loop.
Related Topics
PL.ERR on pg. 1 | PL.ERRFTHRESH on pg. 1 | PL.ERRMODE on pg. 1 | PL.ERRWTHRESH on pg. 1
|
Copyright © 2015 Kollmorgen™ |
|