You are here: Tools > AKD into KAS > Workbench User Guide > AKD Overview Screen

Drive Overview

Once your drive is connected, the Overview shows a summary of the drive that you are using.

You can view or edit the following information from the Overview window.

Button or Dialog Box

Description

Parameter

Name

Names each drive in use with a unique identifier.

DRV.NAME on pg. 1

DriveControl device for regulating the speed, torque and position of a motor Model

Displays the model number of this drive. The model number is also on the label on the side of the drive.

If you are offline, then you can change the type of drive that you are simulating.

DRV.INFO on pg. 1

Drive Type

Selects the operational fieldbus for your drive.

DRV.TYPE on pg. 1

Drive Active

The drive is active when it is enabled and also supplies voltage to the motor.

DRV.ACTIVE on pg. 1

EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive.

Click Enable to turn on the power stage in the drive and apply voltage to the motor. This command may fail for many reasons; see DRV.EN for further details.

DRV.EN on pg. 1

DisableRemoval of the ENABLE signal. Disables power stage.

Click Disable to turn off the power stage and remove the voltage applied to the motor.

DRV.DIS on pg. 1

Drive Display

This graphic replicates the two-digit seven-segment display located on the front face of the drive. The seven-segment display shows a code that indicates the state of the drive and any faults that may be present. WorkBench shows a copy of what the drive display currently shows. A key to the display is here.

 

Blink

Click Blink to force the display to alternate between the whole display being on and the whole display being off for 20 seconds. You can use this button to confirm that you are communicating with the correct drive hardware.

DRV.BLINKDISPLAY on pg. 1

Setup Wizard

The Setup wizard takes you through the essential configuration steps so that you can control the motor movement.

 

More

Click More to display Serial Number, Firmware Version, Cumulative On Time

 

Serial Number

This text box displays the unique serial number of the drive you are communicating with. The serial number is also shown on the label on the side of the drive.

DRV.INFO on pg. 1

Firmware Version

This text box displays the version of the firmware code running inside the drive.

DRV.VER on pg. 1

Cumulative On Time

This text box displays the cumulative time this drive has been powered on. When the drive is powered on, this value continues counting from the value it had when the drive was last turned off.

DRV.RUNTIME on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™