| + Addition | addition |
| - Subtraction | subtraction |
| * Multiply | multiplication |
| / Divide | division |
| - (NEG) | integer negation (unary operator) |
Below are the standard functions that perform arithmetic operations:
| MIN | get the minimum of two integers or an ANY |
| MAX | get the maximum of two integers or an ANY |
| LIMIT | bound an integer to low and high limits or an ANY |
| MOD | modulo |
| ODD | test if an integer is odd |
| SetWithin | Force a value when within an interval |
|
Copyright © 2015 Kollmorgen™ |
|