Sequential Function Chart (SFC) Editor

The SFC"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions Editor is a powerful graphical tool that enables you to enter and manage Sequential FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Chart according to the IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 standard. The editor supports advanced graphic features such as drag-and-drop, so that you can freely and rapidly arrange the elements of your diagram. It also supports automatic chart formatting when inserting or deleting items, and thus enables quick input using the keyboard.

SFC diagram components Related Sections
Steps
Transitions
Divergences
Parallel branches
Jump to a step
Macro steps
Actions
Conditions
Timeout check
 
Using the SFC toolbar
Drawing divergences
Viewing the chart
Printing the chart
Moving or copying parts of the chart
Entering macro-steps
Renumbering steps and transitions
Entering actions of a step
Entering condition of a transition
Notes for steps and transitions
Bookmarks
Program Limitations

For more details on SFC language, also refer to Sequential Function Chart (SFC).

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™