UNIT.VLINEAR

General Information

Type

NV Parameter

Description

Sets the linear velocity units.

Units

N/A

Range

0 to 3

Default Value

0

Data Type

Integer

See Also

VL.FB , VL.CMDU , VL.CMD , MOTOR.TYPE

Start Version

M_01-00-00-000

Description

UNIT.VLINEAR sets the units type for the velocity parameters when the motor type (MOTOR.TYPE ) is linear.

Type

Description

0

CountsInternal count pulses, 1 pulse = 1/2^20turn per second

1

Millimeters per second

2

Micrometers per second

3

(Custom Units) per second

Related Topics

1   Selecting Units for Your Application

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™