UNIT.VROTARY

General Information

Type

NV Parameter

Description

Sets the velocity units when the motor type (MOTOR.TYPE ) is rotary.

Units

rpm, rps, deg/s, radian/s(Custom Units)/s

Range

0 to 4

Default Value

0 rpm

Data Type

Integer

See Also

VL.FB , VL.CMDU , VL.CMD , MOTOR.TYPE

Start Version

M_01-00-00-000

Description

UNIT.VROTARY sets the velocity units when the motor type (MOTOR.TYPE) is rotary.

Value

Units

0

rpm

1

rps

2

deg/s

3

(Custom Units)/s

4 radian/s

Related Topics

1   Selecting Units for Your Application

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™