BODE.FREQ

General Information

Type

R/W Parameter

Description

Sets the frequency of the sine excitation source.

Units

Hz

Range

0 to 8,000 Hz

Default Value

0 Hz

Data Type

Float

Start Version

M_01-00-00-000

Description

BODE.FREQ sets the frequency of the sine excitation source in Hz. The sine excitation source is used to take frequency response measurements of a system.

Example

Setting up a sine excitation source of 0.2 A at 50 Hz:

-->BODE.INJECTPOINT 1

-->BODE.IAMP 0.2

-->BODE.FREQ 50.0

-->BODE.MODE 2

Related Topics

Using the Performance Servo Tuner

Using the Performance Servo Tuner: Advanced

Scope

Settings

F126 n126

Error: Invalid Bode plot mode for this function.

BODE.MODE

BODE.INJECTPOINT

BODE.VAMP

BODE.IAMP

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™