FunctionMLAxisMoveVelPipe Network motion icon

Description

Jog at the specified speed. Returns TRUE if the function succeeded

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Speed

Description

Sets the Axis Speed

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes, after the motion has reached jog speed

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLAxisGenWriteSpd

MLAxisGenWriteDec

MLAxisGenWriteAcc

Previous Function Name

MLAxisRun

Example

See Usage Example of Axis Functions for additional examples.

Structured Text

 

MLAxisMoveVel(PipeNetwork.Axis1, 500 ) ;

 

Ladder Diagram

MLAxisMoveVel: LD example

 

Function Block Diagram

MLAxisMoveVel: FBD example

Go back to the top of the page [Top]

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen