AXIS#.HOME.IPEAK

Description

AXIS#.HOME.IPEAK is the peak current that will be applied when homing against a mechanical stop.

AXIS#.HOME.IPEAK is used when AXIS#.HOME.MODE is 8, 9, 10 or 12.

The current limits AXIS#.IL.LIMITP and AXIS#.IL.LIMITN are set to ±AXIS#.HOME.IPEAK while homing. Once the home position has been found, the current limits are restored before any additional move using AXIS#.HOME.DIST starts.

By default, this value is zero. For the axis to move AXIS#.HOME.IPEAK needs to be set to greater than zero. If AXIS#.HOME.IPEAK is zero and AXIS#.HOME.MODE is 8, 9 or 10, W6026 warning is generated. If the home move is started with this warning, then F6026 fault is generated.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS, using either a PACClosed"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.

Type

Read/Write

Units

Arms

Range

0 to AXIS#.IPEAK

Default Value

0

Data Type

Float

See Also

AXIS#.HOME.MODE

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.HOME.IPEAK 0x5008 0x5 DINT 1000:1 - RW False
AXIS2.HOME.IPEAK 0x5108 0x5 DINT 1000:1 - RW False

Related Topics

Homing

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen