AXIS#.HOME.DIST
Description
After the axis has completed the sequence to find the home position, AXIS#.HOME.DIST allows an additional movement, relative to the new home position. This extra movement allows the axis to move away from the found home position by this distance. A value of 0 will prevent any movement and leave the axis at the found home position.
This additional movement uses the homing acceleration, deceleration, and velocity.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
Type |
Read/Write |
Units |
Depends on AXIS#.UNIT.PROTARY AXIS#.UNIT.ACCLINEAR Rotary: counts, rad, deg, Custom Units, 16-bit counts |
Range |
Depends on units. See Position Range for details. |
Default Value |
0 |
Data Type |
Float |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.HOME.DIST | 0x5008 | 0x9 | DINT | - | Position | RW | False |
AXIS2.HOME.DIST | 0x5108 | 0x9 | DINT | - | Position | RW | False |
Related Topics
Homing