Acronyms
| Term | Definition | Description |
|
AKA |
Also Known As |
Provides an alias to a name. |
|
AKD |
Advanced Kollmorgen Drive |
|
|
AKI |
Advanced Kollmorgen Interface |
|
|
AKT |
Advanced Kollmorgen Terminal |
|
|
ANSI |
American National Standards Institute |
A private, nonprofit organization that oversees the development of voluntary consensus standards for products, services, processes, systems, and personnel. |
|
ASFB |
Application Specific Function Block |
Library that can be written to provide a specific application task. |
|
ASIC |
Application-Specific Integrated Circuit |
An integrated circuit (IC Modern ASICs often include entire 32-bit processors, memory blocks including ROM, RAM, EEPROM, Flash, and other large building blocks. |
|
BiSS |
Bi-directional Serial Synchronous interface |
An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC |
|
CAM |
Computer-Aided Manufacturing |
The use of a wide range of computer-based software tools that assist engineers and CNC machinists in the manufacture or prototyping of product components. |
|
CAN |
Controller Area Network |
A broadcast, differential serial bus standard developed for connecting electronic control units. Each node is able to send and receive messages, but not simultaneously. For more information, see CAN bus. |
|
CF |
Compact Flash |
A mass storage device format used in portable electronic devices. |
|
CIP |
Common Industrial Protocol |
CIP |
|
CRC |
Cyclic Redundancy Check |
A type of function that takes as input a data stream of any length and produces as output a value of a certain fixed size.
|
|
CSV |
Comma-Separated Values |
A file type that stores tabular data. |
|
DMA |
Dynamic Memory Allocation |
Either:
|
|
EDS |
Electronic Data Sheet |
A file format that defines the communication behavior and object dictionary for the devices following the CANopen standard CiA 306. EtherCAT |
|
ENI |
EtherCAT Network Information |
|
|
ERP |
Enterprise Resource Planning |
ERP integrates (or attempts to integrate) all data and processes of an organization into a unified system. |
|
ESI |
EtherCAT Slave Information |
|
|
FBD |
Describes a function between input variables and output variables. A function is described as a set of elementary blocks. |
|
|
Free Form Ladder Diagram |
A method of drawing electrical logic schematics.
|
|
|
FoE |
File over EtherCAT |
Enables access to any data structure in the device.
|
|
FPGA |
Field-Programmable Gate Array |
A semiconductor device configured by the customer or designer after manufacturing. |
|
FailSafe over EtherCAT |
A protocol specified for the transmission of safety relevant data.
|
|
|
GUI |
Graphical User Interface |
A type of user interface people interact with on a computer and computer-controlled devices. |
|
HMI |
Human-Machine Interfaces |
HMIs are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response. Also known as computer-human interfaces (CHI). |
|
IC |
Integrated Circuits |
Miniaturized electronic circuits consisting mainly of semiconductor devices, as well as passive components. They have been manufactured in the surface of a thin substrate of semiconductor material |
|
IDE |
Integrated Development Environment |
An integrated development environment is a type of computer software that assists computer programmers in developing software. |
|
IDN |
Identification Number |
An IDN preceded by the prefix "P", specifies a product specific (manufacturer) IDN in short-hand notation.
|
|
IEC |
International Electrotechnical Commission |
A not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic, and related technologies. |
|
IEC 61131 |
|
IEC |
|
IEC 61131-3 |
|
IEC 61131-3 is the third part of the open international standard IEC 61131.
|
|
IL |
Instruction List |
Is a low-level language and resembles assembly. |
|
IPC |
Industrial PC |
Is the x86 PC-based computing platform for industrial applications.
|
|
IRQ |
Refers to the act of interrupting the bus lines used to signal an interrupt. |
|
|
JTAG |
Joint Test Action Group |
Used for accessing sub-blocks of integrated circuits.
|
|
KAS |
Kollmorgen Automation Suite |
Umbrella name for a software package including the KAS-IDE |
|
KAS-IDE |
Kollmorgen Automation Suite - Integrated Development Environment |
This is the GUI It is a Windows integrated design environment (IDE) containing all the tools and editors (based on the different IEC 61131 languages) users need during the entire life cycle of the machine. |
|
KAS Runtime |
Kollmorgen Automation Suite - Runtime |
This is the engine that provides a soft PLC and a motion controller. |
|
KVB IDE |
Kollmorgen Visualization Builder - Integrated Development Environment |
Kollmorgen Visualization Builder is an editor that allows the end-user to control the KAS Runtime. |
|
LD |
Ladder Diagram |
See FFLD. |
|
LSB |
Least Significant Bit |
Sometimes abbreviated as LSB, the least significant bit is the lowest bit in a series of numbers in binary; the LSB is located at the far right of a string. Example: In the binary number: 10111001, the least significant bit is the far right 1. |
|
MDI |
Multiple Document Interface |
Graphical computer applications with an MDI are those whose windows reside under a single parent window (usually with the exception of modal windows). This is instead of all windows being separate from each other (single document interface). Advantages
|
|
ML |
Motion Library |
This is the interface between the IEC 61131-3 logical application and the motion engine.
|
|
MSB |
Most Significant Bit |
This is the bit position in a binary number having the greatest value. |
|
Modular Device Profile |
The EtherCAT Modular Device Profile defines the data structure organization for a device with subdivided substructures.
|
|
|
NAT |
Network Address Translation |
In computer networking, this is the process of modifying network address information in datagram (IP) packet headers while in transit across a traffic routing device for the purpose of remapping a given address space into another. |
|
NIC |
Network Interface Controller |
A hardware device that handles an interface to a computer network and allows a network-capable device to access that network. |
|
NTP |
Network Time Protocol |
A networking protocol for clock synchronization between computer systems. The PCMM2G can be configured to synchronize with public NTP See Network Time Protocol for more information. |
|
NVRAM |
Non-Volatile Random Access Memory |
The general name used to describe any type of random access memory which does not lose its information when power is turned off.
|
|
OEM |
Original Equipment Manufacturer |
Refers to containment-based re-branding, namely where one company uses a component of another company within its product, or sells the product of another company under its own brand. OEM refers to the company that originally manufactured the product. |
|
OPC |
OLE for Process Control |
The original name for an open standard to specify the communication of real-time plant data between control devices from different manufacturers. |
|
PCI |
Peripheral Component Interconnect |
This specifies a computer bus for attaching peripheral devices to a computer motherboard. |
|
PCMM |
|
Programmable controller used to control multiple EtherCAT slave drives and I/O. Essentially a AKD PDMM without an AKD. |
|
PD |
Programmable Drive |
A Drive can be programmable, which means it has an open hardware and software architecture to make it ready for nearly all conceivable customer-specific modifications Also known as Servo Amplifiers or Servo Drive |
|
PDMM |
Programmable Drive Multi-axis Master |
Programmable drive used to control multiple EtherCAT slave drives and I/O. |
|
Process Data Object |
|
|
|
PID |
Proportional-Integral-Derivative |
A PID controller is a generic control-loop feedback mechanism widely used in industrial control systems.
|
|
PLC |
Programmable Logic Controller |
This is a digital computer used for automation of industrial processes (e.g., control of machinery on factory assembly lines). It is used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators |
|
PNE |
Pipe Network Engine |
The Pipe Network concept is an innovative solution to solve axis synchronization problems. It is based on Pipe Blocks representing the whole mechanical system by analogy. |
|
POU |
Programmable Organization Unit |
A list of programs where the programs are executed sequentially within the target cycle according to the order defined by the user and displayed in the Project View. |
|
Qwt |
Qt Widgets |
A graphics extension to the Qt GUI application framework from Trolltech ASA. |
|
RTC |
Real-Time Computing |
The study of hardware and software systems subject to a real-time constraint (i.e., operational deadlines from event to system response). |
|
RTOS |
Real-Time Operating System |
A multitasking operating system intended for real-time applications. |
|
S300 |
Servostar 300 drive |
See Servo Drive. |
|
S700 |
Servostar 700 drive |
See Servo Drive. |
|
SCADA |
Supervisory Control And Data Acquisition |
SCADA systems are typically used to perform data collection and control at the supervisory level. Some SCADA systems only monitor without doing control, these systems are still referred to as SCADA systems. |
|
Service Data Object |
The SDO protocol is used to read and write values across fieldbuses
|
|
|
SFC |
Sequential Function Chart |
Used to program processes that can be split into steps. The main components are:
|
|
SPLC |
Software version of a PLC |
Usually working on PC-based hardware. |
|
SSH |
Secure Shell Protocol |
SSH is a network protocol for secure data communication and remote command execution. SSH |
|
ST |
Structured Text |
A high-level language which is block structured and syntactically resembles Pascal. |
|
TDI |
Tabbed Document Interface |
Allows multiple documents to be contained within a single window, using tabs to navigate between them. |
|
TMP |
Trapezoidal Motion Profile |
This Pipe Block is a source block that frequently serves as a virtual master for a system composed of several pipes. Generally, a trapezoidal motion profile generator is used to generate a flow of values with a first derivative which produces a trapezoidal trajectory. |
|
UDFB |
User-Defined Function Block |
Used as a sub-Function Block in another program of the application.
|
|
User Datagram Protocol |
UDP is a network protocol used for the Internet.
|
|
|
USB |
Universal Serial Bus |
A serial bus standard to interface devices. |
|
UTF8 |
Unicode Transformation Format (8-bit) |
A variable-length character encoding for Unicode. It is able to represent any character in the Unicode standard, yet the initial encoding of byte codes character assignments for UTF-8 are backward-compatible with ASCII. |
|
UU |
User Units |
A coordinate value or length expressed in user units represents a coordinate value or length in the current user coordinate system. Thus, 10 user units represent a length of 10 units in the current user coordinate system. |
|
XML |
Extensible Markup Language |
XML is a general-purpose markup language. It is classified as an extensible language because it allows its users to define their own tags. |
|
VDK |
Visual DSP Kernel |
Operating system supported by Blackfin microprocessors. |
|
VLAN |
Virtual LAN |
A group of hosts with a common set of requirements that communicate as if they were attached to the Broadcast domain, regardless of their physical location.
|
|
XPe |
Windows XP Embedded |
A componentized version of the Professional edition of Windows XP.
|
|
WUI |
Web User Interface |
WUI is the set of means by which people interact with a particular machine, device, computer program, or other complex tool via the Web. |