Fieldbus - EtherCAT
|
Name |
Description |
|---|---|
|
Reads a drive parameter by sending an ASCII command to a drive. |
|
|
Reads a single drive parameter by sending an ASCII command to a drive. |
|
|
Writes a drive parameter by sending an ASCII command to a drive. |
|
|
Returns a list of bad EtherCAT |
|
|
Performs an action on an EtherCAT device. |
|
|
Provides the EtherCAT state and the port link status information for the EtherCAT device. |
|
|
Returns the EtherCAT device-specific information. |
|
|
Deprecated. |
|
|
Reads the EtherCAT master state and the lost frame counter to determine if EtherCAT is running normally. |
|
|
Reads cyclic parameter (byte offset format). |
|
|
Reads a 32-bit word from I/O nodes using a CANopen SDO read command. |
|
|
Returns the current number of working counter errors for the Sync unit. |
|
|
Writes cyclic parameter (byte offset format). |
|
|
Writes a 32-bit word to I/O nodes using a CANopen SDO write command. |
|
|
Transfers safety parameters from the safety master to safety slave devices to initialize the safety network. |
Remarks
- The client (aka EtherCAT master) is the KAS Runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running application. - The servers (aka EtherCAT slaves) are the drives and I/O nodes where data can be retrieved.
- The SDO function blocks only support the reading and writing of 32-bit values.
- It is the fundamental size of CANopen SDO calls.
Why use ECATReadSdo and ECATWriteSdo FBs?
The ECATReadSDO and ECATWriteSDO response time is faster.
They are preferred over DriveParamRead and DriveParamWrite.
Why use the DriveParam FBs?
Reasons to prefer the DriveParam FBs are:
- They allow direct use of the parameter name.
- Example: IL.LIMITP instead of the SDO index: 356Eh
- They can be used to setup a drive terminal in the HMI
"Human-machine interfaces "
Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response application. - This is similar to the Terminal view available in the AKD widget embedded in the KAS-IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger.
- This is similar to the Terminal view available in the AKD widget embedded in the KAS-IDE