Fieldbus Library
These tables list the Fieldbus
A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design functions and function blocks:
EtherCAT Library
|
Name |
Description |
|---|---|
|
Reads a drive parameter by sending an ASCII command to a drive. |
|
|
Reads a single drive parameter by sending an ASCII command to a drive. |
|
|
Writes a drive parameter by sending an ASCII command to a drive. |
|
|
Returns a list of bad EtherCAT connections. |
|
|
Performs an action on an EtherCAT device. |
|
|
Provides the EtherCAT state and the port link status information for the EtherCAT device. |
|
|
Returns the EtherCAT device-specific information. |
|
|
Deprecated. |
|
|
Reads the EtherCAT master state and the lost frame counter to determine if EtherCAT is running normally. |
|
|
Reads cyclic parameter (byte offset format). |
|
|
Reads a 32-bit word from I/O nodes using a CANopen SDO read command. |
|
|
Returns the current number of working counter errors for the Sync unit. |
|
|
Writes cyclic parameter (byte offset format). |
|
|
Writes a 32-bit word to I/O nodes using a CANopen SDO write command. |
|
|
Transfers safety parameters from the safety master to safety slave devices to initialize the safety network. |
EtherNet/IP (ODVA)
|
Name |
Description |
|---|---|
|
Provides information about the current state of the Scanner connection. |
|
|
Sends an explicit message (UCMM) to an EtherNet/IP adapter for reading a single CIP |
|
|
Sends an explicit message (UCMM) to an EtherNet/IP adapter for reading a single CIP attribute. |