MC_GrpReadActPos
Function Block
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Reads the actual position of the axes in the group.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Enable |
BOOL |
0, 1 |
N/A |
No default |
If TRUE, this function block reads the current actual position of the axes in the group. |
|
AxesGroup |
No range |
N/A |
No default |
The axes group the actual position is read from. |
|
|
CoordSystem |
SINT |
One of these enumeration values:
|
N/A |
No default |
The coordinate system used when reading the actual position. |
|
Position[] |
LREAL |
No range |
User units |
No default |
An array where the position data is written.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Valid |
BOOL |
No range |
N/A |
If TRUE, the positions have been read without error. |
|
Error |
BOOL |
No range |
N/A |
If TRUE, an error has occurred. |
|
ErrorID |
INT |
No range |
N/A |
Indicates the error if Error output is TRUE. See the table in PLCopen Function Block ErrorIDs. |
Remarks
-
-
This function or function block returns cached data.
See Program a Multi-Core Controller for more information.
- See Coordinated Motion, the top-level topic for Coordinated Motion.
- See Function Blocks - General Rules for more information about how inputs and outputs work.
- The MC_GrpReadActPos function block fills the array specified by the Position argument with the actual position of the system in the coordinate system specified by the
CoordSystemargument. - This function or function block does not generate any motion.
-
-
Currently, only the ACS coordinate system is supported.
See Coordinate Systems for more information.
- There is a one-to-one correspondence between the axes in the Axes Group and the position values in the Position Array.
- Each element in the Position Array corresponds to the axis element in the Axis Group array.
- If an index in the Axes Group is unassigned, the position value for that array element in the Position Array is 0 (zero).
- If the element does contain an axis, the position value is filled with the current actual position for that axis.
Figure 6-140: MC_GrpReadActPos
FBD Language Example
FFLD Language Example
IL Language Example
BEGIN_IL
"Instruction List"
This is a low-level language and resembles assembly
CAL Inst_MC_GrpReadActPos( DoRead, Group, CoordSys, PosList )
END_IL
ST Language Example
Inst_MC_GrpReadActPos( DoRead, Group, CoordSys, PosList );
See Also