MLCNVConnectEx
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Connects the output of a pipe to an axis data other than the control position.
Inputs
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
|
|
Returns TRUE if the converter is connected to the Axis object. See Pipe Network - General Rules for more information. |
Remarks
- This function:
- Connects an extra converter Pipe Block to the specified axis.
- Connects several converter Pipe Blocks to the same axis and acts on different data.
- Normally a Converter block sends position values to an Axis.
-
-
This FB does NOT work if you have Simulated the device.
In this instance, the FB continuously generates error messages in the Controller log window.
-
-
Add 16#8000 to the designated IDN number for ValueID input. 8000 in hexadecimal signals a vendor-specific IDN value.
- The PDO
PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. values are overwritten by Mapped PLC variables including either: - A possible link to the mapping of variables.
- The section on MLParamWrite() warning indicating that the function block write of Analog output is overwritten by the MLCnvConnectEx function.
Precedence Rules
- A PLC variable mapped to Analog Output takes precedence
In arithmetic and algebra, when a number or expression is both preceded and followed by a binary operation, a rule is required for which operation should be applied first. From the earliest use of mathematical notation, multiplication took precedence over addition, whichever side of a number it appeared on. Thus 3 + 4 × 5 = 5 × 4 + 3 = 23.
To change the order of operations, we use parentheses (). Thus, if we want to force addition to precede multiplication, we write (3 + 4) × 5 = 35. - If MLCNVConnect assigns a Pipe output to an Analog Output, it takes precedence over a DriveParamWrite function call.
- DriveParamWrite modifies the Analog Output but is overwritten by the higher precedent options if they are present.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Connect a converter Pipe Block named “CNV1” to the pipe block named AXIS1, And send feed-forward (EC_ADDITIVE_TORQUE_VALUE) to the drive
MLCNVConnectEx( PipeNetwork.CNV1, PipeNetwork.AXIS1, EC_ADDITIVE_TORQUE_VALUE, 0 );
See Also